AXIS#.HOME.DEC

Description

This parameter sets the deceleration used while homing.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Range for details.

Default Value

10,000 RPM/s

Depends on units. See Acceleration Units for details.

Data Type

Float
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
AXIS1.HOME.DEC

5008h

07h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.HOME.DEC

5108h

07h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.DEC

6102

17D6

Unsigned32

Read/Write

Acceleration

AXIS2.HOME.DEC

71638

117D

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.DEC

6102

Float

Read/Write

Acceleration

Related Topics

Homing